When reading from the ISM330DLC using I2C, the sensor sometimes stops responding.
Hey guys,
I am working on communicating to an ISM330DLC sensor using I2C and a TI processor as the master. We only have the accelerometer enabled (no gyro) and are using the FIFO to read the data. When the FIFO gets four pieces of data (2 x, 2 y, and 2 z) we receive an interrupt and then read all of the data out of it. This seems to be working, but every now and then the accelerometer stops responding. The issue seems to be completely random and can happen any time, including in the middle of a read. I have seen it happen after only about 10 seconds of collecting data or after about a minute of taking data. The state of the I2C bus seems to vary as well after the error.
I've attached a picture of an example of this happening below. In the picture we were trying to read the FIFO status bits and the FIFO data in one read. It looks like we properly read the status bits and the first half of the data, but then the I2C lines get stuck low in the middle of the read. Everything leading up to this looked perfect.
Does anyone have any idea what could be causing this issue? The bus voltages look pretty good and it seems to be functioning completely normally, until the sensor just stops responding.
Thanks for the help,
Charles