Which pedometer tool functions are avaliable in offline mode of Unico GUI?
I am working on improving the pedometer functionality on a sensortile.box device.
I would like to use the regression tool provided in the Unico GUI, to use pre-recorded data patterns to configure the pedometer.
The problem I ran into is, that if I load patterns into the Debug /Data Injection Tool, they are either not recognized, or the values are 0 or -2147483648 (min value of signed 32 bit int), or the program crashes instantly without error code.
If I use the regression tool on my pattern folder, it does something and creates a .ucf and config file, but no matter what patterns I give the tool, the .ucf is always the same.
The Patterns were tested in the MLC Tool, which accepted them and interpreted them correctly.
The only reason I could think of is, that the extra motherboard is needed in order to use these tools, but I was not able to verify or disprove this assumption, so I would be thankful for an answer to that.
Best Regards,
K. Werner.