"WHO_AM_I register value does not match the device selected"
My first time exploring with STEVAL hardware. I just received the STEVAL-MKI108V3 mother board, the STEVAL-MKI196V1 sensor board, and installed UNICO GUI 9.13.0 and FW Version V3.11.4.
When starting the Unico Program with both "Automatic Port Detection" and "Communication with the motherboard" enabled then selecting MKI186V1 sensor (LSM6DSO), a dialog box appears saying "The WHO_AM_I register value does not match the device selected." Looking at the motherboard and sensor board documentation, there does not seem to be any jumpers for setting device address.
I have verified the orientation of the sensor board into the DIL socket. I believe the LSM6DSO address is either 0x6A or 0x6B, but have no idea what address Unico is looking for. Any suggestions on how to resolve this?
Out of curiosity, with USB plugged into mother board and blue LED is on, I measured the voltage at pin VDD to GND on sensor socket and it is 30mv (expected 3.6v). Is the device powered on automatically by mother board, or is this a fault?
Thanks for any help! Rich