WHO_AM_I values / readout problems
Hi,
I "think" I have a H3LIS331DL (mounted on its back due to hardware issues with the SAMLC21 based prototype and now fixed with glue). I am aware of the obvious changes in accel directions, but just want to get the prototype running. When reading the WHO_AM_I I get the value of 0b10110010 (and not 0b00110010). I am using SPI at 5MHz, MOSI and MISO look fine with MISO going to high on the falling (9th) SCLK edge in preparation of the first bit being a 1.
A test read of the CTRL_REG1 which powers up to 0b00000111 according to the data sheet gives me the value 0b00000111.
Can it simply be a wrong chip? If so: which one?
Anybody seeing similar problems?
Thanks
Frieder