Question
Why AHRS Update rate is 50Hz when STM32 can work at 72MHz ?
Posted on April 06, 2012 at 09:35
I don't understand why AHRS updated only at 50Hz when STM32F103xx can work at 72MHz.
I want to reprogram iNEMO v2 board to change the AHRS update rate to 200Hz. What limits STM32 to update AHRS at only 50Hz.I'm working on designing a AHRS board based on STM32, if STM32 can't update more than 150Hz, i want to drop working on STM32.Thanks. #inemo #ekf-update-rate