Why is LSM6DSL using so much current in power-down?
We are seeing a large current draw when the LSM6DSL is in power-down mode, or low-power mode. The current measured is roughly 120 uA. IC is wired for I2C. We have an identical setup with a LIS3DH that does not have this issue.
Is there a register we need to change? Again , this 120 uA appears when power is supplied to the IC.
LSM6DSL Connections:
SDO: Unconnected
SA0: Unconnected
SDx:
Connected to
GroundSCx:
Connected to
GroundINT1: Floating
INT2: Floating
CS: External pull-up with 10k
SCL: Connected to MCU i2c lines and other I2C devices - External pull-up with 10k
SDA:
Connected to MCU i2c lines and other I2C devices - External pull-up with 10k
#power-consumption #lsm6dsl