Why ranging Time-of-Flight sensor (VL53L1X) gives fluctuate value for fixed distance?
While measuring the distance of an obstacle using VL53L1X ( https://www.st.com/en/imaging-and-photonics-solutions/vl53l1x.html ) the result is fluctuating. This was tested with the breakout board ( https://www.st.com/en/evaluation-tools/vl53l1x-satel.html ).
Example of the test conducted:
We have set the fixed obstacle at a distance of 140 mm from the sensing unit.
Case 1: Setting:
Ranging: Autonomous ,
Distance Mode: Short ,
Timing Budget: 50ms ,
Inter measurement period: 50ms.
Result: Varies in the range 138-144 mm
Case 2: Setting:
Ranging: Autonomous ,
Distance Mode: Short ,
Timing Budget: 500ms ,
Inter measurement period: 50ms.
Result: Varies in the range 139-141 mm
Why the variation is observed for the tightly fixed obstacle (non varying distance) in these kind of sensors? What is the physics behind it (measurement fluctuation reason)? Please help me with the technical explanation.
With regards,
Bhaskar Ghosh