Skip to main content
Visitor II
October 12, 2018
Question

With respect to the RHF1401 Rad Hard ADC, what are the impacts to performance and recovery time of analog input overdrive?

  • October 12, 2018
  • 0 replies
  • 495 views

Case 1: driving the analog inputs out of range but below the absolute max positive value (eg +2.8V)

Case 2: driving the analog inputs negative sufficiently far to engage the input protection diode (eg current limiting input resistor driven to -7V). What is the input protection diode current handling capability? The intention is to include series resistance on the input to avoid damaging transient overdrive. +2.8V, -7V are the possible transient inputs to Vin and Vinb.

    This topic has been closed for replies.