Write issues with CTRL_REG6_XL of LSM6DS0
Hi everybody,
I have a custom board hosting anLSM6DS0 sensor and an STM32F427 micro which communicate via SPI. The SPI interface is configured as follow:
SPI5h.Instance = SPI_MEMS;
SPI5h.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
/* 5 MHz */
SPI5h.Init.Direction = SPI_DIRECTION_2LINES;
SPI5h.Init.CLKPhase = SPI_PHASE_2EDGE;
SPI5h.Init.CLKPolarity = SPI_POLARITY_HIGH;
SPI5h.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SPI5h.Init.CRCPolynomial = 7;
SPI5h.Init.DataSize = SPI_DATASIZE_8BIT;
SPI5h.Init.FirstBit = SPI_FIRSTBIT_MSB;
SPI5h.Init.NSS = SPI_NSS_HARD_OUTPUT;
SPI5h.Init.TIMode = SPI_TIMODE_DISABLE;
SPI5h.Init.Mode = SPI_MODE_MASTER;
At startup I firstly check if the module is present reading successfully the WHO_AM_I register, then I try to configure theCTRL_REG6_XL register to enable the accelerometer. So I perform the following write/read operations
1.
HAL_SPI_Transmit(&SPI5h, &wCTRL_REG6_XL,
sizeof
(rCTRL_REG6_XL), 1000);
2.
HAL_SPI_Transmit(&SPI5h, &diCTRL_REG6_XL,
sizeof
(diCTRL_REG6_XL), 1000);
3.
HAL_Delay(100);
4.
5.
HAL_SPI_Transmit(&SPI5h, &rCTRL_REG6_XL,
sizeof
(rCTRL_REG6_XL), 1000);
6.
HAL_SPI_Receive(&SPI5h, &rxSENSOR,
sizeof
(rxSENSOR), 1000);
7.
HAL_Delay(100);
where
wCTRL_REG6_X = 0x20,
rCTRL_REG6_X =
wCTRL_REG6_X | 0x80 and
diCTRL_REG6_XL = 0x20 is the configuration data. That is, I just switch on the accelerometer leaving every other parameter at default.
At row 5, then I read again the register content to check whether the settings have been correctly stored, but
rxSENSOR = 0xF0. Within the module's reference pdf I could not find anything related with this and I am really puzzled.
Any suggstion is appreciated. Regards.