In the STR710-EVAL board document on page three it says
embedded 1.8 V voltage regulator for core supply (options to use the on-board 1.8 V regulator allows full speed operations, Since there's a starting bracket but no ending one I assume that there are some text missing, or was removed. I cannot find anything in the 'reference manual' saying that a ''better external 1.8V is needed'' So what does this full speed operations mean?
embedded 1.8 V voltage regulator for core supply (options to use the on-board 1.8 V regulator allows full speed operations,Thanx for the clarification /Yxan/