Skip to main content
Visitor II
May 28, 2006
Question

2 UARTS

  • May 28, 2006
  • 2 replies
  • 734 views
Posted on May 28, 2006 at 22:16

2 UARTS

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:09

    Hi All,

    I am working with uPSD3400 and I intend to work with the two UARTs.

    Is it possible to use one timer (TIMER2) for both of the UARTs?

    They are working with the same baud rate and not working at the same time.

    Thanks

    KH

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:09

    Yes, if you set them to operate in mode 1, which is the standard asynchronous mode.

    Han-Way Huang