Posted on November 23, 2005 at 00:13 FLASH_WritePrConfig (FLASH_B1F0,DISABLE); if execute this line,result is: program crash. why? when cpu reset , the register 0x4010dfb0=0xfcfcff00,but in datasheet indicate ''Address offset: 0x10 DFB0h Delivery value: 0xFFFF FFFF Bit 31:18 Reserved, must be kept at reset value (1).'' I don't known whats means.
As the STR71x datasheet the Executing from Flash with RWW is limited with a CPU frequency up to 45 MHz. I hope that this can help you to resolve the problem. Cheers, Hich