Can anyone tell me ,how to access the SRAM reserved for DDC application ( 0xff00 to 0xffff) if we re not using the DDC chanel. I tried to specify in KEIL the XRAM space 0xff00 to 0xffff . but it's showing : '' xadat memory range out of bounds.'' In our application, we are short of variables. , so wee wants to put the large queue in this memory spavce. Purvi
thanks for the reply. I tried that way..but i am not able to read the data back (what i am stroing at power on) it's not able to read that location eg: BL51 locate: pdata: 0xff00 pdata char var-extra3; var_extar3=0x33; put_char_q_tx(var_extar3);
You are right, I have just realised the upsd unlike other 8032 based devices does not have a xram page register, so pdata will not work.
The only other solution is to make sure the xdata you are declaring is in another xram segment, this can be done by declaring the xdata in another file, use data via extern. The keil linker tries to allocate all variables in the same xram segment, this causes problems when you have 2 xram areas. Also remember to enable the ddc xram: MOV A, #60H ; enable DDC XRAM MOV DDCCON, A in your startup file is enough. and the checkbox ''Use On-chip xram ...'' is enabled. Regards sjo