I would verify that I've understood the reference manual correctly. At page 336 it says that the input resistamce of an ADC input (in round robin mode) is: 3000 [kOhm][MHz] /fmod In my application PCLK2 is 32MHz and the prescaling factor set to 500. According to my calculations the input resistance is 47kOhm. Is this correct?
47MOhm was a 'better' value (my fault). That makes it possible to use a lower prescaling factor without getting a redicoulisy low input resistance value. ;) Thanx