Skip to main content
Visitor II
September 8, 2003
Question

ADC temperature conversion

  • September 8, 2003
  • 2 replies
  • 686 views
Posted on September 08, 2003 at 11:39

ADC temperature conversion

    This topic has been closed for replies.

    2 replies

    userAuthor
    Visitor II
    September 5, 2003
    Posted on September 05, 2003 at 17:01

    Hi to all,

    can you send me some example about ADC temperature conversion

    with 10bit ? To reduce space I have thought to use a 256 step temperature conversion table (255=100° 0=0°) ,

    not 1024. Is possible ?

    Many tanks to all

    mbks
    Visitor II
    September 8, 2003
    Posted on September 08, 2003 at 11:39

    I think selecting the range will depend up on your type of thermistor you are using. It is because you may have variation of more than 255 steps when the tempreture will rise from 0-100 degrees because of large change of resistance of thermistance so the input voltage with tempreture.