Skip to main content
Visitor II
February 10, 2020
Question

Add XCUBE-WIFI1 library to project generated via CUBEMX

  • February 10, 2020
  • 1 reply
  • 710 views

Hi,

I have IDW04A1 wifi module and i would like to use it in my project which was generated with CUBEMX, but there is no visible XCUBE-WIFI1 package in the evironment (additional software) and I also cant add it manualy...

How can I add thoese drivers and middleware to my project so i can use wifi capabilites?

    This topic has been closed for replies.

    1 reply

    Visitor II
    February 11, 2020

    I have the same situation, i want to use the idw01m1, but i cannot add the x-cube-wifi in cubemx. :(