we developed a small and flexible in-system-programming-box, which allows to programm the ST9x devices. Simply connected to PC via RS232, it is possible to run scripts for predefined actions, i.e. RESET, FLASH-ERASE, PROGRAMM, LOAD-BOOT-APPLICATION, ... even it is possible to run own small programms in the internal RAM without programming the flash! is anyone interested? email me. regards, siggi
Posted on May 17, 2011 at 11:34we developed this tool cause the ST-programming board is not usable for production und the segger tool is too unflexible. we had another small application, so it was no long way to redesign it as a ISP-Tool for the ST9. It generates the RESET und other ISP-Signals and transfers data from/to the PC via RS232. The PC kann interoperate with a simple script file or manual actions do perform actions: reset erase flash sector erase chipflash donwload hexfile download binfile load your application into ram and execute it the last point is remarkable: you can execute applications without the need of programming the flash! so you are able to test special functions very fast. the tool is connected the the target-system with the 6 lines: +5V/GND/RESET and the ISP-Signals. regards, siggi
Posted on May 17, 2011 at 11:34we designed the tool to get best results for development AND production-use. as mentioned earlier, it is very flexible and therfore for many tasks useful.
Your tool looks good! If you use ISP, you probably need HW between your application and PC? Is it working as the ST programming board? I mean with another micro as a master...?
We tried to contact you directly few weeks ago, but apparantly did not succeed to reach you. We are still interested by getting information on your Programmer. Could you please send us your email via the Contact Us screen on stmcu.com home page. Bye. arnie