On 2003-09-04 16:40, siggi wrote: hi! we developed a small and flexible in-system-programming-box, which allows to programm the ST9x devices. Simply connected to PC via RS232, it is possible to run scripts for predefined actions, i.e. RESET, FLASH-ERASE, PROGRAMM, LOAD-BOOT-APPLICATION, ... even it is possible to run own small programms in the internal RAM without programming the flash! is anyone interested? email me. regards, siggi [LIST][*]null How do I get intouch with you, I don't see any email link ???