Skip to main content
Visitor II
July 6, 2004
Question

Amplifier of the ST7 FLITE05/09

  • July 6, 2004
  • 8 replies
  • 1485 views
Posted on July 06, 2004 at 08:38

Amplifier of the ST7 FLITE05/09

    This topic has been closed for replies.

    8 replies

    Visitor II
    June 16, 2004
    Posted on June 16, 2004 at 06:53

    Hey there,

    I'm trying to use the amplifier of the FLITE05. The range should be 0-250mV. But in this range I got a ADC Range from 9 - 113.

    When I increase the voltage up to 500 mV, the ADC Value increase up to 200 which is the highest ADC result.

    Where is the problem?

    Visitor II
    June 16, 2004
    Posted on June 16, 2004 at 07:10

    I've no experience with the ST7Flite, but i read the datasheet, and i noticed that the range 0-500mV only works if the Vdd is 5V.

    Visitor II
    June 16, 2004
    Posted on June 16, 2004 at 08:15

    My Vdd is 5,1V, but the range is in the data sheet from 0V - 250mV. (Chapter 11.4.3.2)

    Visitor II
    June 22, 2004
    Posted on June 22, 2004 at 14:36

    You are right the input voltage range when Vdd is 5 V is indeed from 0 - 250mV.

    Visitor II
    June 22, 2004
    Posted on June 22, 2004 at 14:40

    You are getting ADC range from 9-113 when the input voltage is from 0-250mV which is right.

    Voutput = Voffset (200mV) + 8*250mV = 2.2V

    Digital value = (2.2*256)/5 = 113

    Visitor II
    July 6, 2004
    Posted on July 06, 2004 at 05:15

    I'm not sure to understand what the problem is, but I see on the note of the chapter 11.4.6 that the amplifier is not available on st7Lite05...

    Visitor II
    July 6, 2004
    Posted on July 06, 2004 at 06:04

    Hi Nico,

    referring to the datasheet the OpAmp isn't available on ST7LITES5 but it is on ST7LITE05.

    Regards

    woro
    Visitor II
    July 6, 2004
    Posted on July 06, 2004 at 08:38

    If you refer page 1 of the datasheet, you would find that ST7Lite05 and ST7Lite09 both have 8-bit ADC with Op-Amp.