I have followed the app note AN1816 for configuring the keil compiler and the psdsoft to handle multi-paged memory. Everything has worked perfectly, but I have had a problem in the last step. Whe it says 'For CSBOOT0, select the same HEX file that you had use for FS0, and set the address range to 0000h-1FFFh. Then click the ok button' if I just make this, it does not work. I need to make the same thing for CSBOOT1, CSBOOT2 and CSBOOT3. Is there any errata on the app note? What am I making wrong? The CSBOOT part is suppossed to be the common part, if I put there the whole ****.H00 code what does it mean? Tahnk you for your attention.
I do not understand your answer very well. What does in mean 'because all is in CSBOOT0'. If I only put there the *.H00 it doe not work. The only way to make it work is putting *.H00 in all the CSBOOTs (CSBOOT0, CSBOOT1, CSBOOT2 and CSBOOT3).