Skip to main content
Visitor II
August 8, 2008
Question

Anglia IDEaliST and Olimex ARM-USB-TINY

  • August 8, 2008
  • 3 replies
  • 814 views
Posted on August 08, 2008 at 05:43

Anglia IDEaliST and Olimex ARM-USB-TINY

    This topic has been closed for replies.

    3 replies

    mykolaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:54

    Hi All,

    I managed to work out a partial answer.

    IDEaliST generates a 'openocd.cfg' file automatically in the project root (I was looking in the IDEaliST install directory beforehand).

    Whenever the debugger gets started, a new 'openocd.cfg' file is generated and overwrites the old one. So hand editing this file is pointless.

    The way I got the debugger working was to untick ''AutoStart Debug Driver when Debugging'' in Debug options, and starting OpenOCD manually in a command prompt with the correct config file.

    I still haven't got the 'Program Flash...' facility going...

    [I might have a good look at Code::Blocks and see if I can get the tools integrated easier???]

    regards,

    Mykola

    mykolaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:54

    Hi,

    I am trying to get Anglia IDEaliST (IDE ver 1.61; Toolchain ver 1.62) with the Olimex ARM-USB-TINY.

    I downloaded the latest openocd (openocd-ftd2xx; svn 717) and managed to get the Jtag hardware recognised and the debugger working (Yagarto).

    I had to do one change and that was to change the PID from 0x0003 to 0x004, and keep VID as 0x15BA. PID of 0x0003 is for ARM-USB-OCD.

    Functioning configuration file attached.

    Now, looking at IDEaliST, there is an (older) version of openocd included. 'olimex-jtag' is available as a hardware option in the GUI, as is necessary. But beyond that, the GUI configuration is limiting.

    Unfortunately I cannot find any configuration file to manually adjust settings (PID, etc).

    Any assistance will be most appreciated.

    regards,

    Mykola

    mykolaAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:54

    Hi,

    I am still getting a ''Hardware Setup Failed, Check Connections'' pop-up (title on pop-up is ''IDEaliST\Plugins\idestr9'') when trying to program the flash.

    Any ideas what the configuration should be?

    Any reasonable documentation for IDEaliST?

    regards,

    Mykola

    PS The reason I am posting here, is that this products has been referred to, and on person is developing for it????