Skip to main content
Visitor II
November 1, 2008
Question

[ANN] eLua (Lua for microcontrollers) 0.5 released

  • November 1, 2008
  • 1 reply
  • 647 views
Posted on November 01, 2008 at 18:23

[ANN] eLua (Lua for microcontrollers) 0.5 released

    This topic has been closed for replies.

    1 reply

    darkoreAuthor
    Visitor II
    November 1, 2008
    Posted on November 01, 2008 at 18:23

    Hi,

    eLua is an open source effort to bring the Lua programming language in the embedded world (MCUs). It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants (STR711FR2 included), as well as Cortex (and i386 as a proof of concept). Version 0.5 was just released, this is the changelog:

    * Added support for STR7 CPUs from ST

    * Added TCP/IP support using the uIP stack

    * Added support for console and shell over TCP/IP instead of serial link

    * Added the ''net'' module (eLua's interface to TCP/IP functions)

    * Added the ''cpu'' module (eLua's interface to the target CPU)

    * New samples: morse.lua (Morse code encoder), lhttpd.lua (Lua scripting HTTP server)

    * Added support for cross-compiling Lua code (compile on PC, run on target)

    * XMODEM can now receive Lua bytecode in addition to Lua source code

    * The XMODEM buffer is now dynamic (grows as needed) instead of fixed size

    * Project documentation updated

    For more details visit the project web page at

    http://elua.berlios.de

    Best,

    Bogdan