Skip to main content
Visitor II
October 13, 2007
Question

any means to program flash using PC serial port?

  • October 13, 2007
  • 3 replies
  • 952 views
Posted on October 13, 2007 at 14:51

any means to program flash using PC serial port?

    This topic has been closed for replies.

    3 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:53

    Hello,

    Can any one has any utility to program the MCU flash using PC serial port.

    Programming using JTAG is not a fissible solution in case of field application.

    In IAP , one can erse the code & program the same if it's from keyboard....but how to program the hex file using PC serial port???

    Any one has any utilty or application code which can send bin or hex file to serial port ????

    Or using hyperterminal, can we send bin or hex file...

    the file size may be of 16Kbyte.

    purvi

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:53

    hello,

    there are so many windows and linux based utility for sending

    hex or bin data to eeprom via rs232 port

    here is one of them

    http://www.lookrs232.com/img/lookRS232.gif

    bye

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:53

    Purvi,

    I use HyperTerminal on Windows and minicom on Linux to do a file transfer using the xmodem protocol. My IAP code/ boot loader code executes from the secondary flash and has a xmodem client. I've written a small utility that converts the hex file to an obj file. So my xmodem client simply writes to main flash whatever it receives.

    I'm not sure if this is the answer you're looking for so if you need more information, please let me know.

    [ This message was edited by: uPSDude on 22-10-2003 23:42 ]