I cant establish a link with the emulator with the board that I've fabricated. I've followed the schematic as in the STR710-EVAL board page 24 of 27. Also, I've probed and checked the connections and layout of the evaluation board and it matches the one in the schematic. The error that is shown is : Target held in reset. Currently, I'm using the JTAG Interface of the evaluation board together with my own fabricated board to communicate and it works perfect! So, any solution for the above problem? Rgrds, ongth60
Im using RVDK 1.6.1 and MB393-2.04. After using the fabricated board to test out the JTAG connection, I can't connect to the evaluation board. :( The error that i received is the same as before : Error : Target held in reset. Warning : Disconnect mode is invalid - ignored. Also, when i tried to configure the connection using Auto Configure Scan Chain, it pops up an error stating Auto configure failed. Check the RVI connection with the target or try using a lower fixed frequency. Rgrds, ongth60
I've tried connecting at lower frequency but failed. Between, i've fabricated and tried three debug boards based on three schematics. The first schematic is based on the schematic of the STR710-EVAL board page 24 except that the transistors i used are tru hole MPS A14 transistors as replacements. Also, the location of the J4 jumper is changed to the recommended location from the AN 1775 page12. I connect the jumper, and when i try to connect the jtag board to the mcu, it will connect but maybe 3 times in 10 tries. So, since the link is not robust enough, i try and modify it by adding a STM811 reset circuit to the jtag board. By then, i cant connect to the emulator and i thought that the jtag board was wrong!! SO...since all the time im using the evaluation board jtag circuit minus the CPU to connect to my fabricated board, which contain the CPU...so i fabricated another jtag board exactly like the one from eval board documentation page 24 except the transistors i used are mps a06. But by then, the emulator should be spoilt already but I didnt knew it until i checked the emulator with another evaluation board, thinking that the emulator was working!! Rgrds, ongth60
Which schematic are u referring to? debug1.jpg or debug2.jpg? By d way if using debug1.jpg I can connect but the link is not robust, I can only connect 2 out of 10 tries!! Btw, I fear my emulator might be spoilt due to the testing. Rgrds, ongth60
My fabricated main board that contains the ARM cpu could worked well with the JTAG board from the evaluation board. I soldered some wires from the JTAG port of the evaluation board to my fabricated main board which contains the ARM cpu. The link is robust and I can connect and disconnect at every instance. The reason I'm using this method is that I can't get a robust link with another JTAG board which I have constructed based on the schematics(debug1.jpg and debug2.jpg) posted above. JTAG board constructed based on debug1.jpg schematic can work but the link is not robust enough. It can connect only 3 times out of 10 times), so I've decided to construct the other JTAG board which contains the reset circuitry based on debug2.jpg.(Pls note that I've changed the transistors) By then, it could nt work well and the errors that I've got are stated above. So, now I've tried to test with a workable evaluation board but my emulator refuse to cooperate. rgrds, ongth60