I have read many message to bank switching and the most correct way to switch is:
Code:
/* prepare bank0 for user operation */ FMI->BBSR = 0; FMI->NBBSR = 6; FMI->BBADR = 0x20000; //0x80000 >> 2 FMI->NBBADR = 0x0; FMI->CR |= 0x18; /* Enable banks 0 & 1 */ Jump_To_Application = (pFunction) BANK0_START_ADDR; Jump_To_Application(); } well this code is correct for switch and now I can look the loader code at address 0x00000000 and the program code at address 0x00080000 but... when i try to access at address 0x00080000 ok 0x00086000 ok 0x00087000 ok 0x00087ffc ok 0x00088000 oh oh i cannot read this why ? this bank is 512kb large :( mumble... mumble.... maybe is better if check the loader in bank 1 0x00000000 ok 0x00006000 ok 0x00007000 ok 0x00007ffc ok 0x00008000 ok OK ??? oh oh... why i can read this ? 0x00008000 is redoundacy of 0x00000000 0x00010000 is redoundacy of 0x00000000 0x00018000 is redoundacy of 0x00000000 0x00020000 is redoundacy of 0x00000000 this bank is 32kb large :( mumble... mumble.... I try to set
Code:
FMI->BBSR = 4; <<<<<<<<<<<<<< Changed FMI->NBBSR = 2; <<<<<<<<<<<<<< Changed FMI->BBADR = 0x20000; //0x80000 >> 2 FMI->NBBADR = 0x0; FMI->CR |= 0x18; /* Enable banks 0 & 1 */ checking....checking.... Wooow Now work fine, very fine the loader writed in 0x00080000 is visible at address 0x00000000 and memory is accessible thru 0x00007ff0 the program code writed in 0x00000000 is visible at address 0x00080000 and is accessible thru 0x000ffff0 Why in all document in this forum and in all example all says this ?