Skip to main content
Visitor II
January 15, 2007
Question

basic EMI Interface question

  • January 15, 2007
  • 2 replies
  • 706 views
Posted on January 15, 2007 at 06:11

basic EMI Interface question

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    Do I need to add an external latch in order to interface the processor to a 1Mx16 SRAM chip?. I know is a basic question, but it seems that the documentation I'm reading suggests that an external latch is not needed: based on ''Insider's guide'' by Hitex (p.54) or on the reference manual (p.37. ''Mux mode with 16-bit data, 24-bit address'')

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    Depends on the device you are connecting to.

    Most Flash/SRAMS will require the external latches as they do not support multiplexed addressing.

    The datasheet of the part you are using will tell you what mode it supports.

    Regards

    sjo