Posted on April 16, 2004 at 11:54TQFP64 package pin 7 is BOOTEN. Does it have any meaning for TQFP64 Can I use pulldown resistor for BOOTEN and forget this pin ? Or is it used for programming ?
we are developing our project in the ST development board STDV710. We want to boot our progrmme from internal flash/RAM. As per the datasheet, in this case we have to use BOOTEN BOOT0 BOOT1 MEMORY 0 X X FLASH 1 0 0 FLASH 1 1 0 RAM in that case can we use the (BOOT0)U0Tx and (BOOT1)U1Tx IN THE UART MODE.