Skip to main content
Visitor II
June 17, 2005
Question

BOOT PIN,S Setting ???????

  • June 17, 2005
  • 1 reply
  • 663 views
Posted on June 17, 2005 at 07:08

BOOT PIN,S Setting ???????

    This topic has been closed for replies.

    1 reply

    zero-bitAuthor
    Visitor II
    June 16, 2005
    Posted on June 16, 2005 at 11:07

    BOOTEN BOOT0 BOOT 1 MEMORY

    0 X X FLASH (Internal)

    1 0 0 FLASH (Internal)

    1 1 0 RAM (Internal)

    1 0 1 System-Memory

    1 1 1 External Memory Bank 0(CS0 AREA : 0x60000000H)

    1) When booting with boot option which is set 1 1 1 according to above, which is prior, CS0 signal or execution of StartupCODE?

    2) In JTAGE DEBUGING MODE, should RAM(Internal) be set to 1 1 0?

    Now debugging is possible although composition of hardware is set to 1 1 1(External flash).

    3) Must V18 Voltage be supplied from external?

    *** My Configreation

    CPU : STR710FZ

    ADS/AXD/MultiICE

    [ This message was edited by: Number2 on 16-06-2005 14:53 ]