Skip to main content
Visitor II
August 10, 2006
Question

button interrupt?

  • August 10, 2006
  • 5 replies
  • 1517 views
Posted on August 10, 2006 at 07:03

button interrupt?

    This topic has been closed for replies.

    5 replies

    mpjAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:31

    Hi,

    Can someone point me to a button interrupt example for the STR910-EVAL board.

    Thanks

    Michael

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:31

    Hi Michael,

    There is an example of button interrupt in the WIU folder in the examples provided with the standard library.

    Best regards,

    STARM

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:31

    hi,

    I found the problem in WIU example

    I need to detect a usb cable removal so I'm trying to use pin P75

    as USB voltage detecting.

    In the example I changed the output pin to P70 and

    when I change the output state the WIU_PR bit related to this

    pin is set.

    The GPIO7OUT is configured as 0x0001

    I'd like to know if this is a normal behavior.

    mpjAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:31

    Thank you.

    Michael

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:31

    Hi,

    I'm trying to use the WIU demo.

    If I contine to press the button the IRQ is always asserted.

    Could you let me know if is possible to assert the irq only

    with a rising or falling edge?