Skip to main content
Visitor II
February 4, 2005
Question

CAD files for STR710 and STR720 Eval Boards

  • February 4, 2005
  • 6 replies
  • 1116 views
Posted on February 04, 2005 at 12:05

CAD files for STR710 and STR720 Eval Boards

    This topic has been closed for replies.

    6 replies

    Visitor II
    January 28, 2005
    Posted on January 28, 2005 at 23:15

    Can someone please supply me with CAD source files for the STR710 and STR720 Eval Boards ? (I presume they were developed using Orcad - most eval boards are ...)

    Visitor II
    January 31, 2005
    Posted on January 31, 2005 at 09:18

    Hello cadrjr,

    Please can you explain ,what does means ''CAD source files ''

    it is a matter of ''gerber'' file or not ?

    With regards.

    Hich :-]

    Visitor II
    January 31, 2005
    Posted on January 31, 2005 at 13:33

    I principly mean the Schematics in Electronic format (ORCAD, etc). (I have them in .pdf format already.)

    Also any Layout files would be useful - files containing the device footprints would save me having to re-enter them all again.

    Gerber files are of no use.

    (The files I need are *.opj, *.dsn , *.olb and *.max if Orcad was used)

    Thanks

    :)

    Visitor II
    February 1, 2005
    Posted on February 01, 2005 at 12:09

    Hello cadrjr,

    Our design engineer use the Mentor tool to develop the Electronic Schematics and Gerber file is the only file we've got.

    Hope that helps.

    Best regards,

    Hich. :p

    Visitor II
    February 3, 2005
    Posted on February 03, 2005 at 04:36

    Hello cadrjr

    You find attached the mentor files attached with this message.

    Hope that helps!

    Cheers

    Hich :p

    ________________

    Attachments :

    mb393a.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht9a&d=%2Fa%2F0X0000000aJh%2F4j_WtyhOPzM2d2Hkj7Wqv3Xp6aGgNt78TQmXdkXN6d8&asPdf=false
    Visitor II
    February 4, 2005
    Posted on February 04, 2005 at 12:05

    Thanks - but these are only Gerber filers for PCB manufacture.