Can I swap D+/- pins on the ECMF4-20A42N10?
The pinout of the connector and USB controller I am using means that I need to flip the differential signals either side of the ECMF4-20A42N10.
The layout would be a lot cleaner if I could swap D+/- signals on this device. For example:
Swap Pins 9/10 and 1/2. So the flow through direction is still the same, but D+/- signals are swapped.
From the representation diagram in the datasheet it appears I can, but I would like to confirm please.
Thanks,
Peter