Skip to main content
Visitor II
May 21, 2006
Question

CAN .sre file for ST10f276

  • May 21, 2006
  • 3 replies
  • 838 views
Posted on May 21, 2006 at 06:21

CAN .sre file for ST10f276

    This topic has been closed for replies.

    3 replies

    dvirAuthor
    Visitor II
    May 18, 2006
    Posted on May 18, 2006 at 04:09

    Hello,

    does anyone know where can i get a sre file for TASKING's CrossView to work with the ST10f276 using ROM-MONITOR through the CAN or the second serial port (XASC) ?

    thanks in advance,

    Dvir :(

    Visitor II
    May 18, 2006
    Posted on May 18, 2006 at 10:55

    Hello Dvir,

    To use the second serial port, you can modify the files c166\mon\serial.c and serial.h accordingly.

    By default, serial port 0 is defined by macro ''PORT'' in file mondef.h.

    To rebuild the ST10276 monitor, goto directory ''c166\mon\mon167'' and run from the command line:

    c166\bin\mk166 clean

    c166\bin\mk166

    To use the rebuilt monitor, copy file m167r.sre to your project directory.

    For more details and clarifications, you can contact TASKING technical support.

    I hope this helps you,

    With best regards,

    Najoua.

    dvirAuthor
    Visitor II
    May 21, 2006
    Posted on May 21, 2006 at 06:21

    hello Najoua,

    thanks for your help, but i was looking for an already made and tested sre file.

    As for Tasking support, they said they don't have the time to write this sre just for one customer.

    thanks and best regards,

    Dvir