Skip to main content
Visitor II
March 5, 2008
Question

Changes to loaded program for in application programming

  • March 5, 2008
  • 5 replies
  • 1061 views
Posted on March 05, 2008 at 15:17

Changes to loaded program for in application programming

    This topic has been closed for replies.

    5 replies

    joshhAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    I am using the in-application programming with uart example and have gotten it working with the example projects provided. However when I loaded a binary of a project that I created it would not run. Is there any special changes I have to make to my project to get it to work with the in-application programmer?

    joshhAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    How do you link the binary file to 0x0? I am using EWARM 4.42.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    Your binary image must be linked to 0x0 and be sure that you have removed the boot bank configuration from the startup file

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    The AN2475 application note contains a pre-configured example. See the following link:

    http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=101

    joshhAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    I have looked over the example project and tried some changes but still can not get it to work with the in-application programmer. So far I have commented this code out of my 91x_init_IAR.s file

    ; --- Remap Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000,

    ; when the bank 0 is the boot bank, then enable the Bank 1.

    LDR R6, =0x54000000

    LDR R7, =0x4

    STR R7, [R6]

    LDR R6, =0x54000004

    LDR R7, =0x3

    STR R7, [R6]

    LDR R6, =0x5400000C

    LDR R7, =0x0

    STR R7, [R6]

    LDR R6, =0x54000010

    LDR R7, =0x20000

    STR R7, [R6]

    LDR R6, =0x54000018

    LDR R7, =0x18

    STR R7, [R6]

    I have also copied over the lnkarm_flash.xcl from the example project to my own. Neither of these has fixed the problem. Is there anything that I am failing to do here? freeRTOS v4.6 is the program I am trying to load.

    [ This message was edited by: joshh on 05-03-2008 20:09 ]