Connection to Bigtreetech SKR V1.4 problems
I am trying to flash a new bootloader to a bigtreetech SKR V1.4 on a 3D printer using a ST-Link V2 STM8/32 and the STM32 ST-Link utility software
When connecting the link to the USB, the power light only lights up on the SKR V1.4 motherboard.
On teh utility app, when trying to "connect to target" I get an error saying it cannot connect and if I am trying to connect to an STM32W1xx device I should select "normal" or "Hotplug" but yet when I do this, I get the same error, saying I should use "connect under reset"
I have triple checked the connections between the link and the SKR V1.4 motherboard and the wire connections all seem to be correct.
I have connected 5 jumper cables: RST, SWDio, gnd, SWClk and 3.3V
I assume the following has something to do with the error but still need help.
As can be seen in the attached screen capture, the "target" is returning a blank field, which says to me the st-link is not connecting with the 3d printer motherboard.
Please assist with a solution if you can.
Thanks
Rob