If I would like to use one GPIO pin as clock source of a pheripheral, that is send 0/1/0/1 sequence on that GPIO pin, anyone know the output data bit rate of it ?
I have some problems with the GPIO's too. I wrote a program only toggeling one GPIO-Pin. The MCLK works with 48 MHz and PCLK1, PCLK2 works with 24 MHz. The toggel-frequency of the Out-Pin is only 146 kHz !! I can't believe that this will be the maximum frequency of a GPIO. What can I do ?