Skip to main content
Visitor II
September 5, 2006
Question

Debug information with JTAG Interface?

  • September 5, 2006
  • 2 replies
  • 701 views
Posted on September 05, 2006 at 11:50

Debug information with JTAG Interface?

    This topic has been closed for replies.

    2 replies

    heribertAuthor
    Visitor II
    September 4, 2006
    Posted on September 04, 2006 at 07:36

    Hello,

    i also have trouble to run the ''B-Programm'' after the IAP initialisation.

    My question: is it possible to view the initialisation and jump to B-MAIN via the JTAG-Interface in any way?

    (I see in program A the jump to B) Is it possible to view the B-program initialisation alone?

    Thanks for help.

    I use IAR and J-Link.

    heribertAuthor
    Visitor II
    September 5, 2006
    Posted on September 05, 2006 at 11:50

    Hello again,

    the IAP Driver (--> Bootloder or B-Program) works fine with connected JTAG Interface and debug mode. I wrote the bootloader with start-and end-address, B-Programm is still in the flash. In standard mode (with or without)connected JTAG Interface it doesn't work. With connected JTAG Interface, after a reconnect the USB plug on the JTAG Interface it runs.

    Only programming B-Programm, so all works.

    Does anyone have an idea, what is wrong?

    Thanks Heribert