Skip to main content
Visitor II
November 25, 2003
Question

DEBUG Interface

  • November 25, 2003
  • 2 replies
  • 656 views
Posted on November 25, 2003 at 18:33

DEBUG Interface

    This topic has been closed for replies.

    2 replies

    jm2Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    Hi!

    I'm designing a PCB with a µPSD3212 - but want to be able to put a µPSD3333 as an option.

    A FLASH-Link Port for the µPSD is designed on the PCB. In addition to the µPSD3212 the µPSD3333 has a ''DEBUG''-pin.

    What to do with this pin to be sure, that I can use the debugging-features? What external hardware do I have to use for debugging? I have the 3200 developement-board and the FLASH-Link-Interface for the printer-port. May I use this for a µPSD3333 as well? Will I be able to archive debugging-features with this?

    Is there already a App-Note for the µPSD3333, that sums up the debugging-features?

    Thanks very much![addsig]
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    Please see the attached, AN1724 , Conversion Guide uPSD3200 to uPSD3300. Also attached, Application note AN1763, has a section on KEIL'S uLink USB-JTAG Debugger used on uPSD33xx.