Skip to main content
Visitor II
May 11, 2005
Question

debugging tools

  • May 11, 2005
  • 4 replies
  • 1042 views
Posted on May 11, 2005 at 08:29

debugging tools

    This topic has been closed for replies.

    4 replies

    ongth60Author
    Visitor II
    May 3, 2005
    Posted on May 03, 2005 at 07:30

    Hi all,

    I would like to ask if the debugger has the ability to record the steps that have been run in the program to trace back the statements that have been executed? Pls advice.

    Rgds,

    TH Ong

    ongth60Author
    Visitor II
    May 3, 2005
    Posted on May 04, 2005 at 00:09

    Hi,

    Thanks for the info. Well,its going to be tough searching for a bug without this functionality.

    Rgrds,

    TH Ong

    ongth60Author
    Visitor II
    May 4, 2005
    Posted on May 04, 2005 at 02:33

    Hi again,

    Does Realview Trace provide the profiler functionality that I've wanted? Im using RealView Ice.

    Rgrds,

    TH Ong

    Visitor II
    May 11, 2005
    Posted on May 11, 2005 at 04:50

    Hi,

    using RealView ICE does not necessarily mean using RVDK, as the JTAG-Adapter shipped with RVDK is referred to as ''RealView ICE Micro Edition''. The RealView ICE is a tool that can be used with RVDS as well, connected to USB or Ethernet.

    @ongth: I guess RealView Trace provides the needed functionality

    regards,

    Marcus