Which tools do support STR750 or STR755 peripherals when debugging?. When I tested it on KEIL MDK-ARM 3.05, the peripherals of simulation debugging is good(but support just GPIO, UART, CLOCK, so on), But the peripherals of real debugging show just STR710's ones not STR750.
How about Hitex or IAR? Are there any other tools which support them? Thanks
I do agree with Zouh, i know that STR750 is fully supported by Keil STR750.nevertheless, Raisonance and Hitex also support STR750 and give you the full access to debug session or simulation with this device. Best regards, MBS ;)