Skip to main content
Visitor II
August 27, 2004
Question

Development Tools

  • August 27, 2004
  • 3 replies
  • 717 views
Posted on August 27, 2004 at 07:23

Development Tools

    This topic has been closed for replies.

    3 replies

    md1Author
    Visitor II
    August 12, 2004
    Posted on August 12, 2004 at 09:16

    Hello,

    I am a little confused over the ordering codes for the ST7MDT20-DVP3 and ST7MDT10-DVP3.

    As far as I can see, if I order an ST7MDT20-DVP, According to the user manual I will get the following:

    A base MEB, a TEB for the 521/321, and an SDIP32 and SDIP42 connectors.

    So if I wanted to work with the TQFP64 (14x14) then in addition to ordering the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also.

    Now, I also want to work with the FLITE devices as well. So I now will order a TEB for my FLITE, because I already have an MEB from the ST7MDT20-DVP. So I will order an additional ST7MDT10-TEB/DVP. My first question is will I get a default DIP16/SO16 kit with the TEB, or will I have to order this seperately? (ST7MDT10-16/DVP).

    My other issue is that in the user guide for the ST7MDT10-DVP indicates that I must specify a connection kit option that accompanies the DVP. Which appears contrary to when ordering the ST7MDT20-DVP?

    Can anybody shed any light on this?

    All the best,

    Marty.
    Visitor II
    August 20, 2004
    Posted on August 20, 2004 at 07:14

    hello,

    >So if I wanted to work with the TQFP64 (14x14) then in addition to ordering >the ST7MDT20-DVP3 I would have to order the ST7MDT20-T64/DVP also.

    Yes

    >So I will order an additional ST7MDT10-TEB/DVP. My first question is will I >get a default DIP16/SO16 kit with the TEB, or will I have to order this >seperately?

    The ST7MDT10-TEB/DVP like the ST7MDT10-DVP3 include by default a DIP/SO package (DIP16/SO16 for ST7MDT10-DVP3)

    >My other issue is that in the user guide for the ST7MDT10-DVP indicates >that I must specify a connection kit option that accompanies the DVP. >Which appears contrary to when ordering the ST7MDT20-DVP?

    the connection option ordering is the same for ST7MDT20-DVP3 & ST7MDT10-DVP3. for example if you need DIP32/S032 you have to order ST7MD10-32/DVP.

    Regards
    md1Author
    Visitor II
    August 27, 2004
    Posted on August 27, 2004 at 07:23

    Thanks Ronaldo.