Skip to main content
Visitor II
August 24, 2016
Question

Discrepancies between eDesignSuite and Datasheet of A6985F5V and A6986F5V

  • August 24, 2016
  • 1 reply
  • 636 views
Posted on August 24, 2016 at 02:05

There are discrepancies between eDesignSuite and datasheet of A6985F5V and A6986F5V.  So I've submitted ST support team for this issue. They said that datasheet is correct. Please refer to TECH022521.

Please correct bandwidth and switching frequecy of eDesignSuite A6985F5V and A6986F5V model.

--------------------------------------Discrepancies-----------------------------------------------------

Datasheet: bandwidth -> less than min(fsw/6, 150kHz)        

eDesignSuite: bandwidth -> less than min(fsw/12, 150kHz) 

Datasheet: switching frequency -> 435kHz                 

eDesignSuite: switching frequency -> 450kHz    

--------------------------------------------------------------------------------------------------------- 

#a6985f5v-and-a6986f5v
    This topic has been closed for replies.

    1 reply

    ST Employee
    August 24, 2016
    Posted on August 24, 2016 at 11:10

    Datasheet: bandwidth -> less than min(fsw/6, 150kHz)        

    eDesignSuite: bandwidth -> less than min(fsw/12, 150kHz) 

    eDesign suggests a little bit more conservative designs, without reaching the theoretical limits of the small signal model.

    Anyway, eDesignSuite also allows to manually modify the compensation network components so that the bode diagram may be estimated with more aggressive designs.

    Datasheet: switching fr

    equency -> 435kHz                 

    eDesignSuite: switching frequency -> 450kHz    

    Thank you. In the next release we will align eDesignSuite to the Datasheet, which is the official reference for the device behavior and parameters.

    Best regards,

    Patrizia Bellitto

    eDesignSuite developers team