Skip to main content
Visitor II
April 23, 2007
Question

Distance with ST7538

  • April 23, 2007
  • 6 replies
  • 1447 views
Posted on April 23, 2007 at 09:19

Distance with ST7538

    This topic has been closed for replies.

    6 replies

    info79Author
    Visitor II
    June 27, 2005
    Posted on June 27, 2005 at 13:42

    I'm tryng to develop a system based on ST7538. I'm in trouble with distance between master station and slave.

    a) Is there any way to simulate distance in power line ?

    b) Which the problems in power lines ?

    c) Shall I comunicate over 1 Km with power line ?

    Thanks for your Help,

    Best Regards,

    Visitor II
    June 27, 2005
    Posted on June 27, 2005 at 15:56

    How are you trying to communicate? Are you using the SPI or the UART peripheral? Which baud rate would you like to select?

    Visitor II
    August 10, 2005
    Posted on August 10, 2005 at 06:07

    The st7538's communication distance is 4-6km

    Visitor II
    August 29, 2005
    Posted on August 29, 2005 at 08:12

    are you sure?

    How do you measure this?

    Visitor II
    April 23, 2007
    Posted on April 23, 2007 at 04:20

    Hi,

    I see a distance of a few hundred meters but with two entities only. As soon as there are more entities on the same network I only get 10-20m.

    E.g. with 30 entities have a max distance of 15 meters. My system is based on 24VAC though, so maybe those values are different for 220VAC.

    Regards

    Reny

    Visitor II
    April 23, 2007
    Posted on April 23, 2007 at 09:19

    Hi,

    Thank you for using STMicroelectroinics products and website.

    This forum is dedicated to ST7 microcontrollers.

    You will get better support by contacting our technical support :

    http://www.st.com/stonline/domains/support/contact_support.htm

    Best regards

    Laurent