Skip to main content
Visitor II
July 26, 2009
Question

download

  • July 26, 2009
  • 1 reply
  • 656 views
Posted on July 26, 2009 at 15:22

download

    This topic has been closed for replies.

    1 reply

    cgerani9Author
    Visitor II
    July 26, 2009
    Posted on July 26, 2009 at 15:22

    Hi everyone,

    I have just received a development board (ARM STM32F103) µ STM32F103RBT6

    With this board, I received some examples. I try to download one of them by RS232 with the software ''Flash loader demo'' in version 1.3.

    I use the project blinky (blinking led). I compile this with Keil µvision3

    and this makes a file blinky.hex.

    With this software of download, I reached to erase the component but at present, it's impossible to download this file ''blinky.hex'' due to a problem of address.

    My parameters are :

    Target : STM32F10xxBxx

    PID (h) : 0410

    version : 2.1

    All addresses are Unprotected

    next

    On one screen

    Download to device :

    c:\Keil\ARM\Examples\Obj\Blinky.hex

    (the adress information is just in read mode)

    next

    Target : STM32F10xxBxx

    Mapfile : STM32F10xxBxx.STmap

    Opretaion : ERASE

    File name : c:\Keil\ARM\Examples\Obj\Blinky.hex

    File size : 128Kb (it's very strange because the capacity of this file

    is only 1581 bytes on the hard disk)

    And the error message is : FAIL : Address not allowed

    Thank you very much for your help

    null