Downloadig Hex or elf file in STM32F103 based BluePill Module
Welcome to everyone!
This question concerns the STM32F103CBT6 microcontroller , I have given a "BluePill" module equipped with this microcontroller. When I download the hex or elf file with STM Programer, it downloads nicely, no problem, But! however, it catches itself without any precedent and locks itself, and a message appears that it is only available in Reset mode, the program meter is no longer connected to the microcontroller. Could this be eliminated somehow, so that whenever I want to download something, can I do it without any problems? There should be no microcontroller "locking", etc. . Thank you very much in advance for your help Everyone!