Skip to main content
Visitor II
November 19, 2003
Question

driving capability (Fan Out ) of the RESETOUT\ Pin ST10F269Z2Qx

  • November 19, 2003
  • 2 replies
  • 703 views
Posted on November 19, 2003 at 11:34

driving capability (Fan Out ) of the RESETOUT\ Pin ST10F269Z2Qx

    This topic has been closed for replies.

    2 replies

    ludgerAuthor
    Visitor II
    November 14, 2003
    Posted on November 14, 2003 at 06:28

    Hi everybody,

    can someone please give me some information about the maximum current, which can be provided by the RESETOUT\ pin of a ST10F269Z2Qx?

    I use the RESETOUT\ pin as an ENABLE signal connected to four AND gates an alredy destroyed three CPUs.

    Visitor II
    November 19, 2003
    Posted on November 19, 2003 at 11:34

    In the specification the output voltage levels Vol and Voh are defined at the respective values 0.45V and 2.4V when the current is 2.4mA. Refer to datasheet DC characteristics section pages 139-140.