Skip to main content
Visitor II
September 24, 2004
Question

EEPROM Emulation Code for uPSD3200

  • September 24, 2004
  • 2 replies
  • 768 views
Posted on September 24, 2004 at 02:34

EEPROM Emulation Code for uPSD3200

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:03

    Hello,

    I use the eeprom emulation code in my application. But I found

    that I have timing problems: If I called eeprom_update() more than

    150 times, the writing time increased continous. At least I took 6 seconds (!)

    to write the data.

    Has anyone notice such a proplem ? Searching throung the linked-list ?

    I'am a little bit confusing how to use the id parameter in

    the functions update_record() and read_record() ?

    Especially if I choose a EEPROM_RECORD_SIZE greater than 1.

    I used the following configuration in eeprom.h:

    typedef enum

    {

    EEPROM_ID_HARDWARE_STATE = 0,

    EEPROM_ID_SECURITY_STATUS = 1,

    EEPROM_ID_TRANSPORT_KEY_BYTE1 = 2,

    EEPROM_ID_TRANSPORT_KEY_BYTE2 = 3,

    EEPROM_ID_TRANSPORT_KEY_BYTE3 = 4,

    EEPROM_ID_TRANSPORT_KEY_BYTE4 = 5,

    EEPROM_ID_TRANSPORT_KEY_BYTE5 = 6,

    EEPROM_ID_TRANSPORT_KEY_BYTE6 = 7,

    EEPROM_ID_TRANSPORT_KEY_BYTE7 = 8,

    EEPROM_ID_TRANSPORT_KEY_BYTE8 = 9,

    EEPROM_ID_LCD_LIGHT = 10,

    EEPROM_ID_POWER_LOSS_STATUS = 11,

    EEPROM_ID_SOUND_VOLUME = 12

    } EepromId;

    // EEPROM Sector size is 8192 bytes

    // EEPROM_RECORD_SIZE and max_records (entered by application /programmer)

    // must be defined such that

    // (max_records * EEPROM_RECORD_SIZE) + header size (7 bytes) <= 8192/2

    // size in bytes of each record

    #define EEPROM_RECORD_SIZE 1

    // number of bytes per sector

    #define SECTOR_SIZE 0x2000

    // maximum number of data records handled in the eeprom emulation

    #define EEPROM_MAX_RECORDS 50

    Ciao, Ciao

    Andreas
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:03

    Please send your questions to the application engineering department at:

    mailto:apps.psd@st.com

    . Also provide the following information so we can better help you:

    Name

    Company Name

    Phone Number

    Location (City, State, Country)

    Production uPSD part number (3234, 3334, etc.)

    Application

    Projected annual volume (units)

    Production start date

    Thanks,

    uPSD Applications Engineering