Skip to main content
Visitor II
May 26, 2003
Question

Elite Local bus and ATAPI

  • May 26, 2003
  • 3 replies
  • 743 views
Posted on May 26, 2003 at 06:54

Elite Local bus and ATAPI

    This topic has been closed for replies.

    3 replies

    havardAuthor
    Visitor II
    May 21, 2003
    Posted on May 21, 2003 at 08:23

    Can I use both ATAPI and Local bus at the same time as ATAPI is on ISA bus?

    Haavard
    Visitor II
    May 23, 2003
    Posted on May 23, 2003 at 11:41

    No. The ISA and Local Bus are mutually exclusive modes of the STPC. They are selected at the time of the boot and therefore cannot be used at the same time.

    Visitor II
    May 26, 2003
    Posted on May 26, 2003 at 06:54

    ATAPI interface is on the PCI bus (not on ISA) and is always available. What is not possible is to have both ISA and Local Bus at the same time.

    Farfalla