Skip to main content
Visitor II
November 3, 2006
Question

EMI with 8Bit/8Bit?

  • November 3, 2006
  • 6 replies
  • 1137 views
Posted on November 03, 2006 at 06:19

EMI with 8Bit/8Bit?

    This topic has been closed for replies.

    6 replies

    thack9Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    Hello!

    We would like to use an external UART with an 8Bit data- and an

    8Bit addressbus. Is it possible to use the EMI in this way?

    In the datasheet on pages 31/32 there is a Fig. 5 that looks the

    right way, but i don't find anything about the usage of port 9

    in this configuration.

    Thanks in advance

    Thomas

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    Hi tomte,

    if you will use an EMI 8 bit non multiplexed mode you have to configure only port 7 which contain the first eight lines of adress.

    Best regards

    mirou

    thack9Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    Hi!

    The multiplexed mode is O.K. for me.

    The question is just: can i use the not used

    (by the UART) address bits (a8..a15) on

    port 9 for gpio's?

    Thanks

    Thomas

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    Hi,

    you need not to use address ,data bus to interface with UART.Any port in input/output mode will be sufficient.You can keep port8,9 in gpio mode and u can use the port to interface with uart.

    thack9Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    O.K.

    Thanks a lot for your help.

    I will try this.

    Greetings

    Thomas

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:33

    Hi tomte,

    please refer to pin description in table4 in the STR9 datasheet. You will see that you can use GPIO9 pins for another function when you configure it in alternate output 1 or its default pin function.

    Best regards

    mirou