Skip to main content
Visitor II
November 8, 2018
Question

EMIF02-USB03F2 D+/D- In Vs. Out?

  • November 8, 2018
  • 1 reply
  • 803 views

If I leave all of the PullUp and PullDown pins disconnected does it matter if the USB Connector side data lines connect to D+/D- OUT while the Controller side data lines connect to D+/D- IN?

This would be the opposite of what is shown in the datasheet but judging by the simplified internal schematic I think it may make no difference.

    This topic has been closed for replies.

    1 reply

    ST Employee
    November 15, 2018

    Dear,

    To withstand 8kV contact and 15kV air discharge, C1 (D+IN) and D1 (D-IN) must be connected to connector, as they withstand these levels, as written on table 1 of datasheet. C3 (D+OUT) and D3 (D-OUT) withstand 2kV.