Skip to main content
Visitor II
July 27, 2006
Question

Emulator clock

  • July 27, 2006
  • 2 replies
  • 578 views
Posted on July 27, 2006 at 10:41

Emulator clock

    This topic has been closed for replies.

    2 replies

    lseletronAuthor
    Visitor II
    July 27, 2006
    Posted on July 27, 2006 at 06:30

    Hi,

    I am using DEV3 emulator. In my program I set bit 1 in MCCSR to 1 to enable Main Clock Output. The problem is that the frequency I measure on this pin is half the frequency I have set in the Debug instruments/MCU configuration box. If I set Fosc to 16MHz I measure 8MHz on the MCO pin, if I set Fosc to 8MHz I measure 4MHz. I checked this with ST7FDALI and ST7LITE.

    Is this the way it should be or not?

    Thanks

    Visitor II
    July 27, 2006
    Posted on July 27, 2006 at 10:41

    Hi,

    Main Clock Output is FCPU which is Fosc/2 (have a look to the clock managment block diagram).

    Then it is normal you get half the frequence you enter.

    This abswer also your PWM problem.

    Best regards

    Laurent